Skip to navigation

The ZED Link Quad is a GMSL2 capture card with 8 GMSL2 ports on two 4-wire FAKRA connectors. It connects up to eight ZED X, ZED X Mini, ZED X Nano, ZED X One GS, ZED X One S, or ZED X One 4K cameras to an NVIDIA® Jetson™ AGX developer kit. The supported multi-camera configurations are described in each setup guide.

ZED Link Quad

Supported devices

Jetson™ deviceGMSL2 SupportGuide
NVIDIA® AGX Orin DevKit✔️Setup Guide
NVIDIA® Xavier AGX DevKit✔️Setup Guide
NVIDIA® Orin Nano DevKit❌-
NVIDIA® Xavier NX DevKit❌-
Other Jetson™ carrier boards-Please contact support@stereolabs.com

Common GMSL2 guides

These guides apply to all the ZED Link GMSL2 capture cards: