Skip to navigation

This page covers humanoids, robotic arms and the data collection setups used to train physical AI models. For each application, it lists the camera, lens, options and host that usually fit, and the pitfalls to avoid. Use these recommendations as a starting point and check them against your requirements.

Before choosing, read the rules that apply to most applications. For a step-by-step selection, see Choose your camera and Choose your ZED Box.

At a glance

ApplicationCameraLensPolarizerHost
Physical AI and humanoid robotsZED X, ZED X One S, ZED X Nano (wrist)Wide or fisheyeDepends on siteZED Box 2 Max
Robotic manipulationZED X Nano, ZED X MiniWideDepends on siteZED Box 2, ZED Box 2 Max
Data collectionZED X Mini, ZED X Nano, ZED XWideDepends on siteZED Box 2, ZED Box 2 Max

For the polarizer, “Depends on site” means: with polarizer outdoors in daylight, without polarizer indoors or in low light. Only the ZED 2i, ZED X and ZED X Mini are available with a polarizer. For details, see Should you choose the polarizer?.

Physical AI and humanoid robots

Humanoid robot walking up a staircase in a city street

Humanoids and other physical AI platforms combine several vision tasks, each with its own camera:

TaskCameraWhy
Navigation, localization and mapping (head or torso)ZED XMid to long range depth, global shutter for accurate geometry during fast motion
Surround awarenessZED X One S with fisheye lens204° horizontal field of view in a 25 x 25 mm camera
Hand and wrist viewZED X NanoDepth from 3 cm, 75 g, 42 x 30.5 mm
Space-constrained heads and faceplatesZED X One SSmallest GMSL2 camera; use two of them for stereo with a baseline from 25 mm

Host: a ZED Box 2 Max. Its Jetson Thor module runs the perception stack and large AI models side by side, and it connects up to eight GMSL2 cameras.

A single ZED X One provides images and inertial data only: depth requires a stereo camera or a pair of ZED X One. The ZED X Nano is designed for indoor use, has no IP rating and does not support body tracking.

Robotic manipulation

Robotic arm with a ZED X Nano on the wrist, picking up an object

Robotic arms, pick-and-place, depalletization and bin picking.

  • Eye-in-hand (camera on the wrist or end effector): ZED X Nano. Its ideal range of 0.05 m to 1.5 m covers the approach and grasp phases, and its 75 g weight suits the wrist.
  • Eye-to-hand (camera above or beside the workspace): ZED X Mini with wide lens, ideal range from 0.1 m to 4 m.
  • Larger workspaces: ZED X, whose 120 mm baseline keeps the depth accurate at longer working distances.
  • High resolution at short range, or a custom depth of field: two ZED X One cameras as a virtual stereo rig. The no-lens versions accept your own optics.
  • Host: a ZED Box 2, or a ZED Box 2 Max when the robot runs large AI models on board, such as learned manipulation policies.

For accurate grasping, check the depth accuracy of the chosen camera at your working distance in the specification pages.

Data collection

Two robot grippers with a ZED X Nano on each wrist and a ZED X Mini between them

Collecting synchronized image, depth and inertial datasets, for example to train AI models, for imitation learning, or for offline analysis.

  • Cameras: choose them by viewpoint, as for robotic manipulation and physical AI. For example, a bimanual teleoperation setup can combine a ZED X Mini for the global scene view and one ZED X Nano on each wrist for the close-range gripper view.
  • Synchronization: GMSL2 cameras connected to the same deserializer capture their frames within 15 µs of each other, so the views of a multi-camera dataset match in time.
  • Host: a ZED Box 2, which records several GMSL2 cameras with the hardware video encoder of its Jetson Orin NX module. Choose the ZED Box 2 Max when the same device also runs heavy AI processing.
  • Storage: plan the storage for the duration of your sessions. The ZED Box Mini has a 256 GB SSD, and the ZED Box 2 and ZED Box 2 Max are available with up to 2 TB.

The exposure and gain settings are applied to the recorded images, so set them for the recording conditions. Record a short test in the real environment first.

Need help?

Contact support@stereolabs.com with a description of your application: working distances, motion, environment and number of cameras.