Skip to navigation

ZED Isaac™ ROS 3 Integration Overview (Legacy)

Open in ClaudeOpen in ChatGPT

This is the legacy documentation for NVIDIA® Isaac™ ROS 3.2 (ROS 2 Humble, Ubuntu 22.04, JetPack 6). It is kept for existing projects and is no longer updated.

For new projects, use NVIDIA® Isaac™ ROS 5 and follow the current Isaac™ ROS documentation.

NVIDIA® Isaac™ ROS (Robot Operating System) is a collection of NVIDIA® CUDA®-accelerated computing packages and AI models designed to streamline and expedite the development of advanced AI robotics applications.

image

ZED ROS 2 Integration

The ZED ROS 2 Wrapper automatically integrates the ZED stereo cameras with the NVIDIA® Isaac™ ROS framework, enabling developers to leverage the power of NVIDIA GPUs for real-time perception tasks.

NITROS Support

When building the ZED ROS 2 Wrapper packages, the build system automatically checks for the presence of the NVIDIA® Isaac™ ROS packages, in particular the isaac_ros_nitros package. If detected, the ZED Camera ROS 2 components are built with NITROS support enabled. NITROS (NVIDIA® Isaac™ Transport for ROS) is a technology that accelerates ROS data streaming by leveraging GPU memory, allowing high-performance data transfer without routing through the CPU.

You can find more information about NITROS and how it works with ROS 2 in the official NITROS documentation.

If the isaac_ros_nitros package is not detected during the build, the ZED ROS 2 Wrapper will still compile and function normally, but NITROS acceleration will not be enabled. You can continue to use your ZED cameras in a standard ROS 2 environment, though you will not benefit from the enhanced data transfer and performance optimizations provided by NVIDIA NITROS.

image

The ZED ROS 2 Wrapper can leverage NITROS thanks to its strong integration with CUDA processing using the isaac_ros_managed_nitros package.

In particular, the ZED ROS 2 Wrapper uses Managed NITROS publishers to publish images and depth maps directly from the GPU memory, avoiding unnecessary data copies and CPU overhead. This results in significantly improved performance for applications that require high throughput and low latency, such as real-time object detection, mapping, and navigation.

The Managed NITROS publisher and its counterpart, the Managed NITROS subscriber, enable efficient, GPU-accelerated data transfer between the ZED camera node and other Isaac™ ROS nodes. Thanks to ROS 2 Type Adaptation, these components maintain compatibility with standard (non-Isaac™) ROS 2 nodes by automatically converting data to standard ROS 2 message types when needed, for example to visualize images in RViz2. This seamless integration ensures high performance while preserving interoperability within the ROS 2 ecosystem.

image

You can find more information about CUDA with NITROS and how it works in the “CUDA with NITROS” documentation.

Get Started

To use the ZED ROS 2 Wrapper with NVIDIA® Isaac™ ROS, you need to install the NVIDIA® Isaac™ ROS packages and configure the environment to support the ZED cameras through the ZED SDK.

Install NVIDIA® Isaac™ ROS with ZED support and NITROS

Follow the instructions to install the NVIDIA® Isaac™ ROS packages and enable the ZED ROS 2 Wrapper with NITROS support.

Tutorials and examples

You can find a variety of tutorials and examples to help you get started with the ZED ROS 2 Wrapper and NVIDIA® Isaac™ ROS integration:

  • NITROS Subscriber: Learn how to create a ROS 2 component that subscribes to the ZED camera’s image and depth streams using NITROS in an Isaac™ ROS node.
  • AprilTag Detection: Learn how to use the ZED camera with the AprilTag detection package in an NVIDIA® Isaac™ ROS environment.