Skip to navigation

GNSS Antenna

Open in ClaudeOpen in ChatGPT

The u-blox GNSS Multiband Antenna (u-blox ANN-MB-00) is an active multiband antenna for the optional GNSS module of the ZED Box. Its multiband reception supports RTK, for centimeter-level positioning with the ZED SDK Global Localization module.

u-blox GNSS multiband antenna

Specifications

FeatureValue
Modelu-blox ANN-MB-00
TypeActive multiband GNSS antenna
Frequency bandsL1 and L2/E5b/B2I
ConstellationsGPS, GLONASS, Galileo, BeiDou
Ingress protectionIP67
Cable5 m RG174 coaxial cable
ConnectorSMA
Dimensions60.0 x 82.0 x 22.5 mm

Compatibility

DeviceAntenna
ZED Box with GNSS moduleConnect the antenna to port 5, on the side of the ZED Box. See Using GNSS with ZED Box.
ZED Box 2 Max with GNSS optionNot needed: two multiband GNSS antennas are included with the device.

The Wi-Fi antennas of the ZED Box do not work as GNSS antennas.

The GNSS module needs the antenna to have a clear view of the sky to get a fix. The GNSS Overview explains how to mount the antenna on your vehicle or robot.