ZED X Driver Release Notes
New features, improvements and bug fixes of every ZED X Driver release
This section lists the changes made to the ZED X Driver in every release, from 1.0.5 to the latest 1.5.0. Each page covers one minor release, with its patch releases listed newest first.
Download links, organized by platform (ZED Link capture card, ZED Box model, third-party carrier board) and by Jetson™ Linux (L4T) version, are available on the ZED X Camera Drivers page. Older packages are available in the driver archive. To install or upgrade the driver, see Install and Upgrade the Drivers.
The driver for the ZED Link MIPI Quad used with the NVIDIA® Holoscan Sensor Bridge on a Jetson AGX Thor™ has its own version numbers. See the Holoscan Driver release notes.
Find the installed version
The version is part of the name of the installed package: