ZED X Driver
The ZED X Driver is the NVIDIA® Jetson™ Linux (L4T) driver package that runs the ZED X family of cameras (ZED X, ZED X Mini, ZED X Nano, ZED X One GS, ZED X One 4K and ZED X One Core). It configures the deserializer of the capture card, the cameras and their IMU, and installs the zed_x_daemon service. The ZED SDK relies on it to open any GMSL2 or MIPI camera connected to the Jetson.
Each package is built for one platform (ZED Link capture card or ZED Box model) and one Jetson Linux version; recent Jetson Linux versions also have a package for the real-time (RT) kernel. Download the package matching your setup from the ZED X Camera Drivers page of the StereoLabs website. The same page also lists compatibility drivers for third-party embedded computers certified by StereoLabs.
Install and upgrade
- ZED Link GMSL2 capture cards: ZED Link Mono, Duo and Quad.
- ZED Link MIPI Quad on a Jetson AGX Orin™ devkit.
- ZED Box series: the driver comes preinstalled. See the GMSL page of your ZED Box to reinstall it after a system upgrade.
Release notes
- ZED X Driver Release Notes: new features, improvements and bug fixes of every GMSL2 and MIPI driver release.
- Holoscan Driver: release notes of the driver for the ZED Link MIPI Quad on a Jetson AGX Thor™ with the NVIDIA® Holoscan Sensor Bridge.