Holoscan Driver
Release notes of the driver for the ZED Link MIPI Quad with the NVIDIA Holoscan Sensor Bridge
The Holoscan Driver runs the ZED Link MIPI Quad on an NVIDIA® Jetson AGX Thor™ through the NVIDIA® Holoscan Sensor Bridge (Lattice), with up to two ZED X One Core cameras over Camera-over-Ethernet. It is released separately from the ZED X Driver and has its own version numbers.
Download links are available in the Holoscan section of the ZED X Camera Drivers page. To set up the camera, see the Jetson AGX Thor setup guide, and the Holoscan troubleshooting section if no camera is detected.
1.0.0
Released: Nov 16, 2026
New Features & Improvements
- Initial support for the Holoscan Sensor Bridge (Lattice) on Jetson AGX Thor with JetPack 7.2. The ZED X One Core is opened from the ZED SDK with
sl::INPUT_TYPE::HOLOSCAN, available from ZED SDK 5.5. See the ZED SDK 5.5 release notes.