Skip to navigation

Using the Sensors API

Open in ClaudeOpen in ChatGPT

The Sensors API lets you access sensors available on ZED depth cameras and perform a wide variety of sensor-related tasks explained below.

Getting Sensors Data

The data from the different sensors are accessible with the SensorsData class. The class contains raw and calibrated values of each sensor.

To retrieve sensor values synchronized with the image frames, you will need to:

  • Open the camera and grab the current image.
  • Get sensor data corresponding to this image using TIME_REFERENCE::IMAGE.
  • Retrieve data from the different sensors.
// Create and open the camera
Camera zed;
zed.open();
SensorsData sensors_data;
// Grab new frames and retrieve sensors data
while (zed.grab() == ERROR_CODE::SUCCESS) {
zed.getSensorsData(sensors_data, TIME_REFERENCE::IMAGE); // Get frame synchronized sensor data
// Extract multi-sensor data
SensorsData::IMUData imu_data = sensors_data.imu;
SensorsData::BarometerData barometer_data = sensors_data.barometer;
SensorsData::MagnetometerData magnetometer_data = sensors_data.magnetometer;
// Retrieve linear acceleration and angular velocity
float3 linear_acceleration = imu_data.linear_acceleration;
float3 angular_velocity = imu_data.angular_velocity;
// Retrieve pressure and relative altitude
float pressure = barometer_data.pressure;
float relative_altitude = barometer_data.relative_altitude;
// Retrieve magnetic field
float3 magnetic_field = magnetometer_data.magnetic_field_uncalibrated;
}

Time Reference

The function getSensorsData can be called with a TIME_REFERENCE. Use TIME_REFERENCE::IMAGE to get the sample closest to the last grabbed image, or TIME_REFERENCE::CURRENT to get the most recent sample available. To get every IMU sample received between two images, call getSensorsDataBatch() after each grab().

To choose the right method and align IMU samples with images, read the Sensors Time Synchronization section.

Retrieve New Sensor Data

To retrieve updated sensor data, getSensorsData must be called at a frequency at least equal to the sensor data rate, using TIME_REFERENCE::CURRENT. Since sensors have different frequencies and their data is stored in the same sensors_data structure, some sensor data might not be updated between two calls to getSensorsData.

To know if a given sensor data has been updated, we compare their timestamps which are used as unique identifiers. If they are the same, then the sensor data has not been updated.

Timestamp last_imu_ts = 0;
while (!exit_app) {
// Call this loop faster than the IMU rate, independently of grab()
zed.getSensorsData(sensors_data, TIME_REFERENCE::CURRENT);
// Check if a new IMU sample is available
if (sensors_data.imu.timestamp > last_imu_ts) {
cout << "Linear Acceleration: " << sensors_data.imu.linear_acceleration << endl;
cout << "Angular Velocity: " << sensors_data.imu.angular_velocity << endl;
last_imu_ts = sensors_data.imu.timestamp;
}
}

Accessing Raw Sensor Data

The Sensors API lets you read raw data from the depth camera’s built-in motion and position sensors. To retrieve raw data, use the uncalibrated values present in sensors_data structure.

Identifying Sensors Capabilities

Sensors factory parameters can be accessed through the API. They cannot be changed as they are fixed in the microcontroller firmware of the cameras. You can access the following parameters:

  • Sensor Type
  • Sampling Rate
  • Range
  • Resolution
  • Noise Density
  • Random Walk (if applicable)
  • Sensor Units
// Display camera information (model, serial number, firmware version)
auto info = zed.getCameraInformation();
cout << "Camera Model: " << info.camera_model << endl;
cout << "Serial Number: " << info.serial_number << endl;
cout << "Camera Firmware: " << info.camera_configuration.firmware_version << endl;
cout << "Sensors Firmware: " << info.sensors_configuration.firmware_version << endl;
// Display accelerometer sensor configuration
SensorParameters& sensor_parameters = info.sensors_configuration.accelerometer_parameters;
cout << "Sensor Type: " << sensor_parameters.type << endl;
cout << "Sampling Rate: " << sensor_parameters.sampling_rate << endl;
cout << "Range: " << sensor_parameters.range << endl;
cout << "Resolution: " << sensor_parameters.resolution << endl;
if (isfinite(sensor_parameters.noise_density)) cout << "Noise Density: " << sensor_parameters.noise_density << endl;
if (isfinite(sensor_parameters.random_walk)) cout << "Random Walk: " << sensor_parameters.random_walk << endl;

Code Example

For a code example, check out the Getting Sensor Data tutorial.