ZED Isaac™ ROS Integration Overview
Use ZED cameras with NVIDIA Isaac ROS 5 through the ZED ROS 2 Wrapper
NVIDIA® Isaac™ ROS (Robot Operating System) is a collection of NVIDIA® CUDA®-accelerated computing packages and AI models designed to streamline and expedite the development of advanced AI robotics applications.
This section explains how to use ZED cameras with NVIDIA® Isaac™ ROS 5 through the ZED ROS 2 Wrapper.
Are you using Isaac™ ROS 3.2 with ROS 2 Humble? Refer to the legacy Isaac™ ROS 3 documentation.
Supported versions
Isaac™ ROS 4.x is not covered by this documentation.
What changed with Isaac™ ROS 5
Isaac™ ROS 5 is a major release that changes how the ZED ROS 2 Wrapper integrates with the Isaac™ ROS packages:
- ROS 2 Lyrical replaces ROS 2 Humble. All the Isaac™ ROS packages, and the ZED ROS 2 Wrapper, must be built for ROS 2 Lyrical on Ubuntu 24.04.
- NITROS was removed. The
isaac_ros_nitrosandisaac_ros_managed_nitrospackages no longer exist. NVIDIA replaced them withrosidl::Bufferand buffer backends, a native ROS 2 Lyrical feature that lets accelerated nodes exchange standard ROS 2 messages. - Fast DDS or Zenoh is required. The buffer backends are supported by the
rmw_fastrtps_cppmiddleware, the default, and byrmw_zenoh_cppv0.10.5 or newer. With other middleware implementations, such asrmw_cyclonedds_cpp, the data published by the Isaac™ ROS nodes does not reach the subscribers running in other processes. See Middleware requirement. - The Isaac™ ROS CLI manages the environment. The
isaac-roscommand replaces therun_dev.shscript and supports three isolation modes: Docker, Virtual Environment, and Bare Metal.
What this means for ZED cameras
- The ZED ROS 2 Wrapper publishes standard ROS 2 messages (
sensor_msgs/msg/Image,sensor_msgs/msg/CameraInfo,sensor_msgs/msg/PointCloud2, …) that Isaac™ ROS 5 nodes subscribe to directly, without any NITROS bridge. The ZED color images use thebgra8encoding, or thebgr8encoding when thevideo.enable_24bit_outputparameter istrue: when an Isaac™ ROS node requires a different encoding, such asrgb8, add the Isaac™ ROS image format converter as shown in the ZED test. - Starting with v5.6.0, the ZED ROS 2 Wrapper supports the
rosidl::Buffermessage fields of ROS 2 Lyrical and publishes the images, the depth maps, the confidence maps, and the point clouds with the CUDA zero-copy transport: the nodes that accept thecudabuffer backend read the ZED data directly in GPU memory, without copies, and all the other nodes automatically receive standard CPU data. Thegeneral.buffer_backendparameter of the ZED Stereo Node and of the ZED Monocular Node controls this behavior:cuda(default) orcpu. Older versions publish the data from CPU memory. - The
.../nitrostopics of the Isaac™ ROS 3 integration are no longer available. - Intra-Process Communication (IPC) is enabled automatically because NITROS is not installed. You no longer need the
enable_ipc:=falselaunch argument, and you can load the ZED node and the Isaac™ ROS nodes in the same container for efficient intra-process data exchange. IPC subscribers receive CPU data: to receive the ZED data in GPU memory, disable IPC as described in the CUDA zero-copy image tutorial.
Get started
- Install NVIDIA® Isaac™ ROS 5 with the Docker or the Bare Metal installation path, and test the installation. Optionally, replace Fast DDS with Zenoh.
- Use ZED with Isaac™ ROS: add the ZED SDK and the ZED ROS 2 Wrapper to your Isaac™ ROS environment, and verify that an Isaac™ ROS node processes the ZED images.
- Set up the CUDA zero-copy transport: learn how the ZED data reach your accelerated nodes directly in GPU memory, then follow the tutorials for images and point clouds.
- Detect objects with Isaac™ ROS: run the RT-DETR or YOLOv8 object detection on the ZED images, with the image kept in GPU memory from the ZED SDK to the TensorRT inference.